This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210反激输出高压,不正常

Other Parts Discussed in Thread: TPS40210

使用TPS40210,反激输出,设计输入12V,输出350V,在偶然的时候,成功输出过正常的电压,但持续的时间不长,芯片就保护了。

通过调节W1,可以调节输出电压,在大部分时候,输出只能到75V左右,再高芯片就自动保护不工作了。

因为曾经输出过350V,所以电路基本原理是正确的,应该处于一个临界状态。有没有大哥知道,这是什么问题?

开关频率调整过,但是不论是调高还是调低,效果都一样,不知是什么问题。

请高手不吝赐教