我用tps61023将3.7V 10000mAh的锂电池升压到5V。空载时测得输出电压为5V。接上负载后输出电压为2.5V,并且电路中得电感L6啸叫。将锂电池供电换为5V的USB供电时,输出能正常带动负载。请问这是什么原因?具体电路如下图所示。电路中的电感L6是1uH 1A的电感,请问是否是电感的额定工作电流太小了导致的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用tps61023将3.7V 10000mAh的锂电池升压到5V。空载时测得输出电压为5V。接上负载后输出电压为2.5V,并且电路中得电感L6啸叫。将锂电池供电换为5V的USB供电时,输出能正常带动负载。请问这是什么原因?具体电路如下图所示。电路中的电感L6是1uH 1A的电感,请问是否是电感的额定工作电流太小了导致的?