LM51551在sepic的应用下面,输入端2~18V电池供电转输出9V供电,输出功率在13W左右,当芯片的输入端低于3V的时候发现芯片输出变成8V左右而且这个8V无法带正常负载.是芯片的功能达不到,还是应用有问题呢?请帮忙review,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM51551在sepic的应用下面,输入端2~18V电池供电转输出9V供电,输出功率在13W左右,当芯片的输入端低于3V的时候发现芯片输出变成8V左右而且这个8V无法带正常负载.是芯片的功能达不到,还是应用有问题呢?请帮忙review,谢谢!
你好,我补充一下这个电路的问题;
1、这个电路现在入口电压为6V时可以启动工作,当电压跌落到4V时也可以工作,进一步跌落到3V后就不能工作了;此时耦合电感入口的电压在2V多一点,因为前级经过了一个二级管的压降,此时的现象是进入了hiccup打嗝模式,PWM波变得稀疏,SS引脚有三角波在不断尝试启动;当电压进一步上升到5V之后就能继续正常工作了;我们需要在电压跌落到3V后还能正常工作;
2、一开始怀疑是电流检测电阻太大,把R1381电阻换成一个5毫欧还是不行,把电流检测电阻R1381直接对地短路,当入口电压跌落到3V时依然会进入到Hiccup电流保护模式;不知道LM51551是从哪里检测到的发生了过流;
3、BIAS和UVLO/EN引脚可以排除,当耦合电感的输入使用可调电源,BIAS和UVLO/EN使用恒定电压源的时候,还是会出现电压跌落到3V就出现过流保护的情况,测试时实际的负载只有0.5W左右;
4、在电压跌落到3V出现Hiccup保护时,PGOOD信号也在不断地拉低拉高,形成了一个方波的波形;
5、在电压跌落到3V出现Hiccup保护时,VCC引脚的输出稳定在6.8V左右,从示波器上看,是一个稳定的输出,没有出现波动;
6、如果断开R1379,就是CS电流检测引脚悬空,当入口电压跌落到3V之后,输出直接跌落到0V,没有输出了;
7、从PWM开关波形来看,当正常输出时,PWM波形是比较密的,当电压跌落到3V出现Hiccup过流保护后,PWM波形变得很稀疏,感觉是时通时断;
按照手册的说明,当BIAS=VCC时,为2.97V至16V;实际使用的BIAS与VCC不是连接在一起的,不适用此标准;BIAS是单独供电的;
当BIAS电压大于等于3.5V时最小升压电压为1.5V,我理解Sepic电路也是类似于升压的原理的;现在BIAS是单独供电的,当入口电压下降时,BIAS电压始终为9V。