This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5005输出-16V的问题

Other Parts Discussed in Thread: LM5005

您好:

       我在使用LM5005芯片将+24V转换成-16V电压时遇到了问题,烦请看到的工程师帮我解答。问题如下:

       在焊接好LM5005及其周围的元器件后,初次上电时,用万用表测量,显示可以正常输出-16V的电压,再次上电时,用万用表测量电压变为-4.5V左右。检查了周围的元器件没有发现问题。下图是我的原理图和PCB,原理图参考的是WEBENCH Power Deisigner中的电路。

图1为我的原理图,设计参数是输入+24V,输出-16V1A

图1

2为贵司WEBENCH Power Deisigner中的电路我的原理图中元器件的参数与这个基本一致,肖特基二极管参数略有差别。

图2

3为我的PCB上的LM5005部分

图3

4为接了50R的负载时测量的-16VGND间的波形,可以看到直流有效值仅为-5.13V

图4

5为接了50R的负载时测量的LM5005SW引脚处的波形,图6至图9均为该图放大后的波形。

图5

图6

图7

图8


图9