This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS61086参数计算的疑问

上图为数据手册11和12页的公式

从公式出现顺序上看,标注的公式3是最先出现的,但是其中的DELTA L是由标准的公式2计算出的。

在标注的公式2中,电感L是变量,是由标注的公式1计算得到的。

步骤1.因此在计算参数时,是否应首先根据标注公式1计算电感量,在计算电感量时可以设定最大电流Iout数值,即可根据系统的输入电压、设计升压输出电压、开关频率及效率这些常量计算出电感量L;

步骤2.根据标注公式1计算出的电感量L,可由标注公式2计算出DELTA L;

步骤3.计算出DELTA L后,可由标注公式3计算出Iout(max)。

我的疑问是:

第一,上述计算顺序是否正确;

第二,在步骤1中假设了需要的最大电流,然而在步骤3中还会计算出Iout(max),两个地方都计算除了最大电流值,这该怎么理解呢?从3个公式的相互关系可以看出,步骤1中假设的电流Iout越大,步骤3中计算出的Iout(max)就会越小。

  • Hi
    按照你提的顺序其实是很混乱的,按照一般boost 的方式来算即可。
    首先确认电感的纹波电流,例如输入功率*n=输出功率计算输入电流,电感的纹波电流是输入电流的0.35倍。然后用你标识的第二个公式来算电感即可。至于你提到的第三个公式只是用于计算最大输出电流,不要在意其顺序。