This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boost电路UCC28019芯片不工作的问题求助

Other Parts Discussed in Thread: UCC28019

最近用UCC28019做一个24Vac转36Vdc的Boost电路,用的是UCC28019,电路完全按照datasheet来搭建,参数用了Ti提供的计算工具来计算,做成电路后芯片完全不工作,不知道是为什么。希望有高人出手相助,感激不尽! 

原理图和PCB图在下面。

输入是220V工频经过可调的隔离变压器降压成24V输入整流桥(用了4个1N4007自己搭的,没有用整流堆),再进入主电路里。

电感是自己绕的,大概200uH;MOS管用了IRF540,DS两端的二极管实际上没有接。

测了芯片的几个管脚电压:7脚VCC供电12V正常;2脚ICOMP测得4V以上,应该是芯片进入了Fault状态后自己输出的;4脚VINS电压1.4V左右,但即便调大了交流输入使其大于1.5V后芯片依然不工作;6脚VSENSE测得3V左右,调整Rvsense2时其电压会变化,并没有固定在5V不变;

(另外,用示波器的探头和地分别接在负载两端时实验室会跳闸,好像是由于示波器是三脚插头,和变压器共地了,所以没有想到用什么办法测各点的波形。。。。。。)