This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DCDC芯片TPS54383PWPR参考电压的疑问

公司设计一款产品中使用到了TI的DCDC电源芯片TPS54383PWPR,根据数据手册设计应用电路如下

发现左边一路5V输出正常,右边一路3.3V输出不正常,实测为3.95V,烧了单片机,FB2脚为芯片参考电压,实测为0.95V,理论上应该为0.8V。后将C62电容,容值改为33uF,输出为3.3V,但是DCDC芯片发烫严重,请问有人遇到过这种情况吗?跪求指导

  • Hi
    chargepump电容只能用33nF左右(建议小于100nF, Datasheet是22nf~82nf), 这个电容用大了,会增大charge电流,造成较大的功耗,并且有烧芯片的风险。
    你的电路和datasheet一致,之所以测试偏高应该是输出不稳定造成的(你可以用示波器确认,万用表不准确)。而造成不稳定的原因很可能是layout不好,建议你比较3.3V和5V的layout差异,或者参考datasheet.
  • 谢谢指导,我们这边后来将R101由原来的20K改为16K得到输出电压3.3V,目前新发现一个现象,在3.3V输出和GND之间增加若干电容,发现3.3V电压降到了2.8V,我想再请教一下3.3V这一路输出对容性负载的大小有要求吗?
  • 若干电容是加了多大的电容,电容越大,意味着电路的环路带宽约窄,环路可能不稳。很可能你的2.8V输出已经不稳了,你可以用示波器看下SW和Vout波形,看是否正常