This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用LM3478制作 15V到75V升压电源。负载电流值不够的问题。

Other Parts Discussed in Thread: LM3478, TPS61040

使用LM3478制作开关电源。15V升75V 但是输出电流不能满足额定输出电流。不能达到20mA。电路图如下:

请问。负载电流除了和电感的值有关系,和RCOMP&Ccomp以及开关频率以及R12 RISEN都有什么关系呢?为什么输出20mA都不能达成呢?PCB如下:

电感使用的是5mm功率电感,额定电流800mV。 二极管额定电流1A.反向电压200V.MOS Vgd=250V,电容使用的是1812的陶瓷电容。负载2.5K功率电阻时,电路会出现吱吱的叫声。电感发出来的。

  • 看一下COMP点的波形,有声音应该是环路存在震荡,补偿参数不合理。
  • Hi
    15V升压到75完全不用升压加chargepump,直接升压即可。 而且可以选择一些比较简单的方案例如内部MOS升压+chargepump(内置MOS会存在电压不够的问题,外置如你选择的LM3478可以直接升压)。或者用内置MOS升压芯片加耦合电感也行。
    例如:www.ti.com.cn/.../slva245.pdf 找15V供电的芯片或直接用TPS61040, 15V通过三极管和稳压管做个5V给芯片。
    这款芯片TI还提供的一个高压方案,是通过SW脚驱动一个外部MOS,是的其升压超过28V的方案也很适合(但现在没有了,下周到公司我可以给你),或者外部增加2级别chargepump也行。
    对于上面LM3478, 首先你需要将并在电感上的电容C21去掉,它可能与电感产生震荡导致电感发出声音。
    其次将C27/28至少增加到4.7uF看看,1uF太小。其次就是补偿要确认一下,你参数上应该不合理。