1.频率可以通过外部RC设置,占空比是怎么调节的?
2.引脚VFB的功能主要是什么,是不是可以控制该引脚的电压大于2.5芯片不工作,小于2.5芯片工作,该引脚只能控制芯片的两种状态,工作和不工作,这样理解对不对?请教各位!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.频率可以通过外部RC设置,占空比是怎么调节的?
2.引脚VFB的功能主要是什么,是不是可以控制该引脚的电压大于2.5芯片不工作,小于2.5芯片工作,该引脚只能控制芯片的两种状态,工作和不工作,这样理解对不对?请教各位!!!
Hi
FB是反馈输入,外部信号与芯片内部基准做比较,然后误差输出。
占空比取决于输入电压,输出电压,变压器匝比以及反馈,所以改变反馈是可以调节输出的,但是不建议大范围调节,因为补偿是固定的。
你可以看看这个文档: www.ti.com.cn/.../getliterature.tsp
vfb是反馈输入信号,与基准电压2.5v作比较,大于2.5v时 comp输出的电压是多少?小于2.5v时,comp的输出电压是多少?
当vfb点的电压从0到2.5v变化时,此时comp点的电压怎么变化?输出占空比怎么变化?
芯片内部两个二极管的管压降是多少?当1v稳压管的电压小于1v时,输出怎么变化 ?
像tl494,占空比输出的决定因素有个时序图,从时钟开始到最后占空比输出,有明显的的推导过程,请问3843有没有类似的资料?