输入用3.7V锂电池,TPS78230输出3V,EN脚接VIN,产品待机功耗2uA,最大峰值电流50mA左右。
待机时,发现输入电压从3.6V增加到4.1V时,功耗也会随之增加,会增加几个uA。
看了下手册,输入电压变化时,静态电流基本不变。
EN脚在5.5V输入电压时最大才40nA,可忽略不计。
Ground pin current在待机2uA电流情况下,功耗应该也增加不了多少吧?IOUT = 150 mA时才8 μA。
增加的功耗与LDO有没有关系呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输入用3.7V锂电池,TPS78230输出3V,EN脚接VIN,产品待机功耗2uA,最大峰值电流50mA左右。
待机时,发现输入电压从3.6V增加到4.1V时,功耗也会随之增加,会增加几个uA。
看了下手册,输入电压变化时,静态电流基本不变。
EN脚在5.5V输入电压时最大才40nA,可忽略不计。
Ground pin current在待机2uA电流情况下,功耗应该也增加不了多少吧?IOUT = 150 mA时才8 μA。
增加的功耗与LDO有没有关系呢?
输出悬空,功耗0.4uA。Iout=1.5uA时,功耗1.9uA。两种情况电压增大,功耗都没有变化,输入电压5V时输出电压最大也就3.02V左右。
我们的产品上,如果输入4.1V情况下,LDO输出能达到3.1xxV。
LDO输出悬空状态,电压增加功耗没有增加。我在输出端接了2M电阻负载,电压增加,功耗也没增加。
是不是证明产品功耗的增大和LDO没有关系?产品待机也才2uA。