TI工作人员你好,
我按照TPS63020评估板去画电路,并且参数选择也一模一样。评估板是输入1.8——5.5V,输出3.3V
在实际测试的时候,我输入2.7V左右的时候,输出是3.3V 但是随着我输入增加,输出也在增加,无法稳定在3.3V。
并且,大概在输入到4V的时候,电感突然响起,然后芯片就烧了。(在测试过程中始终是空载情况 )
请问为什么会发生芯片烧坏这样的情况。我的电感也是1.5UH 并且满足大电流4A电感。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.