但18页应用举例中又写可以通过1MΩ上拉到12V输入上。我的设计中直接将EN/UVLO通过1MΩ上拉到12V,使用一段时间后发现有约20%的器件发生失效,无电压输出。请问是否由于管脚过压导致?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
但18页应用举例中又写可以通过1MΩ上拉到12V输入上。我的设计中直接将EN/UVLO通过1MΩ上拉到12V,使用一段时间后发现有约20%的器件发生失效,无电压输出。请问是否由于管脚过压导致?
Hi
EN阻抗指的是失效芯片EN管脚对地阻抗吗?
输入端有使用示波器测量过,测出会有电压过冲,大概20V持续25ns
Hi
芯片开封后用显微镜观察发现基板上标的是TPS25923A1,请问这是否正常,还是我们买到翻新芯片了?
你好,
Mark应该是259240,可以申请些样品看看,谢谢。