各位大神好:
参考TI网站上UCC2897A的一个应用例子PMP5426做了一个电源。变压器自己绕制,原边,副边,辅助绕组变比为6:4:4,其他器件值与PMP5426相同,但是贴了几块之后发现,有的板子可以正常工作,有的无输出,测量是2897AVDD引脚电压只有11.23V,即BAIS输出11.23v,几个板子都是11.23V左右,测量D4,D7,L2,C13均正常,找了好久没有发现问题.谁能给个建议,谢谢了。其中一块正常的板子在把2897A拆掉重新装上之后也成11.23V了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位大神好:
参考TI网站上UCC2897A的一个应用例子PMP5426做了一个电源。变压器自己绕制,原边,副边,辅助绕组变比为6:4:4,其他器件值与PMP5426相同,但是贴了几块之后发现,有的板子可以正常工作,有的无输出,测量是2897AVDD引脚电压只有11.23V,即BAIS输出11.23v,几个板子都是11.23V左右,测量D4,D7,L2,C13均正常,找了好久没有发现问题.谁能给个建议,谢谢了。其中一块正常的板子在把2897A拆掉重新装上之后也成11.23V了。
HI
如果手头有电感,可以先将1mH的电感换小点点,主要要电流要足够(规格书上是60mA,但我觉得饱和电流建议大一点看看)
将辅助绕组多绕1到2圈看看?
谢谢,我试试将电感减小一点试试,辅助绕组多绕过,没有效果
谢谢你这么耐心地解答啊。但是之前做的有可以正常工作的,而且有一块板子是好的,但是我把2897a拆了又装上就不行了,这是为啥啊?
你好:
能说下用的哪种互感器么?我有几个启动不了的换了2985好了......但是这样成本太高了,而且不适合大规模量产