This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B6950,搭建的电源模块商用汽车电控单元是否可用

Other Parts Discussed in Thread: TPS7B69-Q1

TPS7B6950是一汽车级芯片,输入电压推荐范围为4V-40,输出5v,其搭建的电源模块是否可以应用在24V系统的商用汽车车身电控单元中?

  • Hi
    这是一款LDO,如果输入电压24V, 在启动瞬间,实际电压会高出24V, 但不能超过40V。 同时看你的负载,如果会超过100mA, 那么功耗会在2~3W, 甚至更高,这对于芯片散热将是一个很大的问题,你需要考虑。 此时更加建议用DC/DC。
    如果实际上,应用电压24V比较稳定,5V输出电流非常小,那么功耗很低的话,可以用这个芯片汽车级版本TPS7B69-Q1.
  • 你好!电压24V电压主要是蓄电池供电,5V输出仅给单片机和CAN芯片供电,且用的LDO芯片是汽车级版本TPS7B69-Q1。
    是否可在TPS7B69-Q1芯片的前端加上一电阻分压?
  • Hi
    如之前所说,你需要确认功耗,和启动瞬间24V是否会有过冲,这个将决定你能够用TPS7B69-Q1.
    你讲的电阻分压在给到LDO供电吗? 这个会因为高边电阻限流的,不能这样用。
    为什麽不考虑DC/DC,因为layout空间不够吗?
  • 您好,这款芯片本就是汽车级的,且是输出5V的,输入电压推荐范围为5.5V-40V,输出电流最大150mA,输出5V供单片机和CAN芯片用,我认为它是可行的,这款汽车级芯片。而且产品已经量产,装车15000量份,车身模块电源部分无问题。请问为什么老建议用DC/DC?
  • 您好,这款芯片本就是汽车级的,且是输出5V的,输入电压推荐范围为5.5V-40V,输出电流150mA,输出5V供单片机和CAN芯片用,我认为它是可行的,这款汽车级芯片。而且产品已经量产,装车15000量份,车身模块电源部分无问题。请问是否有隐患?