This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL783输出电压不正确

Other Parts Discussed in Thread: TL783

我使用两个TL783组成电流源输出。电路如下:

第一个TL783(U4),根据手册给的输出电压计算公式Vo=Vref x (1+R2/R1);得到的输出Vo应该=96.7V,然而,实际情况如图中标注的电压所示,随着输入电压的升高输出电压也升高,并不是输出一个恒定的电压值。

我的设计初衷是:让U4的输入输出压差在15V左右,根据手册说明,这样U4就能提供700ma左右的电流给U3,U3作为恒流源,就可以调整U3的外接电阻R,根据手册提供的公式I=Vref/R,U3j就可以提供700ma以内的我们想要的恒定电流了。

  • 芯片在不同电流情况下, Dropout电压不同。700mA情况下,室温下,Dropout电压是13V左右。也就是U4要保证你目前设定正常输出电压时,输入电压在110V以上。你测试时,输入电压是多少?

  • Hi
    从给的电压看输入输出差压维持3V左右,芯片已经损坏,你需要确认输入是否因为layout, 导线引起的spike, 或者有硬开关震荡等导致输入电压超过125V引起芯片损坏。
    应用上如上面所提到,输入输出必须保持足够压差,否者电压会偏低的,偏高一般是芯片损坏。
  • 感谢您的回复!

    假设U4的输入输出按照Dropout曲线,压差有15V左右,也就是说保证U4具有提供700ma的能力,按照我提供的电路U3U4的连接方法,有一下三问:、

    1、U3U4的连接结构是不是组成了电流源结构?

    2、如果是电流源结构,根据手册提供的公式I=Vref/R,可以调节R的值,U3j就可以提供700ma以内的我们想要的恒定电流了,对吗?

    3、如果是电流源结构,我设定的U4输出是97V,测量的U3输出95V左右,稍微有些压降,U3的电压输出现象是正常的吗?