用户要求电源上电后为关机状态(电源无输出),当后台发命令后,再开机.
实现方式可否通利用输入过压检测脚.
将VREF通过两个电阻分压的方式接到输入过压检测脚上,
正常上电后,电源输入过压检测脚.上电阻分压后的电压大于1.27V,使电源处于输入过压状态,无输出.
开关机信号通过光耦隔离,当要求开机时,光耦次级导通,将OV脚对地的电阻短接,OV脚电压低于1.27V,电源开机.
如何插入图形
谢谢.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题是控制信号的供电与2897A的供电同步,等控制信号过来之前,2897A的输出就会有一下。然后再关的情况。这对用户来说是不可接受的。
这个属于软起动的一种,如果D5\D9\R4\C23,在输出达到设定值之前,TL431不工作,光耦的原边没有电流,无法调整占空比,但有这个电路,只要有输出,就会通过R13、光耦、D5给C23充电,也就是有电流流过光耦原边,提前调整占空比,当环路稳定后,通过R4将C23充电到输出电压,这样不会影响环路的稳定性,当关机后,C23通过D9快速放电,为下次软起动做准备。具体表现你可以看看这个帖子。