Hi 你好,
附件是我们产品上使用的POE电路,带的负载为8W左右,产品24小时运行,试产1000pcs,有9pcs在运行中POE损坏,全部为TPS23753APW的GATE脚对地短路,其推动的MOSFET无损坏,对比好片与损坏的芯片,VC引脚对RTN引脚的阻抗无变化。请问能否给一些解决这个这个问题的指引呢? BTW,这个电路我们在前代产品有使用,其后端功率为5W,量产后POE年损坏率在千分之3左右。
William1464.POE.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi 你好,
附件是我们产品上使用的POE电路,带的负载为8W左右,产品24小时运行,试产1000pcs,有9pcs在运行中POE损坏,全部为TPS23753APW的GATE脚对地短路,其推动的MOSFET无损坏,对比好片与损坏的芯片,VC引脚对RTN引脚的阻抗无变化。请问能否给一些解决这个这个问题的指引呢? BTW,这个电路我们在前代产品有使用,其后端功率为5W,量产后POE年损坏率在千分之3左右。
William1464.POE.pdf
Hi,
有测量过,我稍后更新VDD1和VC的波形上来。
VC正常工作是的电压再12V左右,如果将Gate与mos断开,可以看到Gate会有一个约19V的过冲,如果正常连接就无法看到。
MOS使用的是FDS2582 ID=2.6A @ 100C Vds=150V Vgs=20V Ciss=1290pF 详见附件。FDS2582-D.pdf
我有一个疑问是目前我们在Gate与MOS之间串接的电阻式33欧姆,这个值是否偏小?
William
Hi,
发现一个可能的原因,但是从理论上没有想明白。
请参看前面贴子上传的原理图,在副边输出电容C356(470uF)后级,我们接了一个LC滤波电路(L10 2.2uH , C357 470uF)。主开关MOS的D极电压Vspike的正常值为85V,我们有几台不良品,这个Vspike峰值达到186V,相应的VC会被推到60V,这样很快就把TPS23753A烧毁。 当我们拆掉上面说的2.2uH电感后,电路恢复正常,更换C356也可以恢复正常,相比之下拆掉L10的修复效果更好,但实际测量C356和L10的参数并没有什么异常。
如果直接拆掉C356,则可以持续复现上述状态,所以我理解大概率的输出电容不良引致,那么如何解析输出电容不良导致原边Vspike过分升高呢? 是因为L10的缘故变相增加了漏感吗? 请指导一下。
以下是正常的波形
以下是不良的波形