ucd9248的1号通道的B分通道的控制端我没有使用,此时DPWM-1B, SRE-1B悬空,FLT-1B接地。把电压信号连接到CS-1B是否会有问题,能否测试这个电压信号,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ucd9248的1号通道的B分通道的控制端我没有使用,此时DPWM-1B, SRE-1B悬空,FLT-1B接地。把电压信号连接到CS-1B是否会有问题,能否测试这个电压信号,谢谢。
The Current Sense (CS) pins on UCD9248 receive a small voltage that is proportional to the amount of current going through the power stage. They cannot be used for measuring output voltage.
If they are not using Ch1-B, they should ground CS-1B.
The output voltage of the power stage being controlled by CH-1A is measured by the EAp1 (V+) and EAn1 (V-) pins.