请教一下各位,最近在用BQ24133这款芯片,输入外部电压是12V,想给12.6V的锂电池充电(3节18650电池串联),按照手册CELL引脚接到VREF上。发现在接上电池之后,没有充电电流。当电池不接时,LED灯常亮。尝试调节输入电压到5V时,LED闪烁,7V时LED常亮。焊接没问题
SW 为10.55V,
VREF为3.3V
ACDRV为18.328V
然后接上电池时,没有变化,电流只有75mA。电池电压我量过是10.77V。以下是电路图。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教一下各位,最近在用BQ24133这款芯片,输入外部电压是12V,想给12.6V的锂电池充电(3节18650电池串联),按照手册CELL引脚接到VREF上。发现在接上电池之后,没有充电电流。当电池不接时,LED灯常亮。尝试调节输入电压到5V时,LED闪烁,7V时LED常亮。焊接没问题
SW 为10.55V,
VREF为3.3V
ACDRV为18.328V
然后接上电池时,没有变化,电流只有75mA。电池电压我量过是10.77V。以下是电路图。