This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS53647 + CS95472Q5MC 常温工作时出现CS95472Q5MC 芯片输出引脚内部短路问题。

Other Parts Discussed in Thread: TPS53647

各位TI专家你们好!

我是ADVA  opitcal networking 一名硬件设计人员。

在我的板上有使用到TPS53647 + CS95472Q5MC 4相输出 1.0V 最大负载电流是80A给Broadcom交换芯片核电压供电。目前我们陆续发现有5片板子出现了常温工作在没有跑业务时负载电流为40A,出现输出对地短路后经过排查发现其中一个CS95472Q5MC 的VSW引脚和芯片自身的PGND短路。 MOSFET管表面有安装heatsink并且 MOSFET在进风口有风扇吹风。

请各位TI专家们赐教:

1)我们之前有拿 5套整机在高温65度 满载业务(通过 I2C读取得到的电流是76A左右) 跑48小时,没有出现过MOSFET短路问题。

2)目前出现问题的是在常温25度不带业务的情况下(通过 I2C读取得到的电流是40A)左右,通过 I2C读取8dh寄存器得到温度的值是36度。同样是在25度不带业务出现有CS95472Q5MC 短路问题。

3)CS95472Q5MC 对安装heatsink有没有要求?CS95472Q5MC 表面能够承受的压力是多大?

4)负载为40A时在CS95472Q5MC  的VSW引脚测得 尖峰电压是19.1V ,尖峰电压持续时间是1ns。

5)导致CS95472Q5MC芯片输出短路的可能的因素有哪些?

6)在提问题单中是否可以上传原理图附件?

谢谢各位!