This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS63061输出电压输出为0V、4.8V、15V输出

Other Parts Discussed in Thread: TPS63061

需要设计一款使用4节(1.5V*4颗)5号电池的电源升降压5V电源,但在测试的过程中发现输出电压与设计完全对不上。测试输入的电压是锂电池(3.3~4.2V),然后输出就变成了15V的电压。多做了几颗进行测试,但是都不在稳定在5V,基本都是在4.8V输出或者没电压输出。以下是电路图及PCBLAYOUT图

  • hI
    电路是参考datasheet的没有问题,通过阻抗测量,确认一下焊接,包括反馈电阻的测量,这个决定输出电压。
    其次注意你用的是饱和电流足够的功率电感,测试是先轻载测试确认?
    另外请问你的芯片哪里买的?
  • 查看了TPS63061的DATASHEET发现里面的参考电路少了个FB的引脚,故没有留意其TPS63061也需要把这个引脚拉高(参考了仿真参考电路),在焊接元件的时候留空了位置。今天重新调整电路之后把FB引脚接0欧姆电阻拉高之后整个电路就正常工作了。折腾了一两天总算是折腾出来问题出在哪了。

    官方DATASHEET参考原理图:

    官方仿真软件原理图: