This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用UC3854B配置700WPFC

Other Parts Discussed in Thread: UC3854B

你好,我第一次做PFC電路,我使用TI的UC3854B來配置大約700W的PFC

輸出電壓385V

開關:SCH2080KE

SiC二極體:H2S060H004

開關頻率設置300K

變壓器採用MAGNETICS的0077440A7鐵芯一次側繞65圈1.2mm線徑,二次側繞4圈0.mm線徑,電感量250uH,感值降幅15.3%

因為之前遇到二次側電壓不夠的問題,因此我現在目前暫時用電源供應器輸出20V來給UC3854B當作電源

目前遇到最大的問題是在重載時效率非常差,效率大約只有80%,輸出電壓有定住在Vrms 380V,Vgs的波形看起來也沒問題

我測試在輕載時的效率是和我模擬結果非常接近的大約88%,照理來說重載的效率應該要比較高,想請問是有哪裡我沒注意到的地方嗎?

藍色線為輸出電壓,黃色線為Vgs

謝謝