使用TPS92692,输入DC20-28V,脉冲式输出:50V、5A,周期3Hz,占空比15%(50ms)。请问TPS92692可以做到这样的功率吗? 在数据手册中并没有看到92692的极限功率是多少,但是使用WEBENCH Designer设计时,显示tps92692无法实现上述功率,原因是电流超出限制。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用TPS92692,输入DC20-28V,脉冲式输出:50V、5A,周期3Hz,占空比15%(50ms)。请问TPS92692可以做到这样的功率吗? 在数据手册中并没有看到92692的极限功率是多少,但是使用WEBENCH Designer设计时,显示tps92692无法实现上述功率,原因是电流超出限制。
今天我测试时发现奇怪的现象。使用外部PWM驱动。当PWM2变为高电平后,PDRV电平跳变,SS电压与COMP电压开始上升,且COMP电压高SS电压0.7V左右(二极管压降),但是GATE驱动却延后了4ms左右才发出。造成现在LED电流只能达到3.5A左右,就出现过压保护。
期间我测试了Iadj信号,2.93V,无异常情况;输入24V,无异常情况;Vref与VCC正常,无异常情况;后来我分析可能是斜率过补偿,分别更换Slope电阻为110K、348K,没有明显的变化。将SS电容由10nF变为100nF,没有明显的变化;断开光源,做过压保护测试,正常,保护电压57V。
希望专家帮忙分析下,谢谢