This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS65251芯片测试中的一些问题

Other Parts Discussed in Thread: TPS65251

Hi,

我在用TPS65251芯片做测试的时候遇到了几个问题。我的测试电路是开环情况下芯片switch的能力,因此LX脚直接接了750欧姆的电阻,另外并联了100k的电阻和0.1uf的电容进行电压监控。FB输入0.8V保持switch on,comp输入0.6V(可调)调节占空比。      

            

现在三路输出都存在一定的问题。正常输出应该是高频方波,buck1的问题是输出电压有0.7V左右的抬升

     

buck2的问题比较严重,输出为10ms左右一个脉冲波

      

buck3的方波有一个比较严重的振铃

请帮助分析一下谢谢!