This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于LM5035的半桥电源上电就烧次级整流MOS和初级电压分压不均问题。

Other Parts Discussed in Thread: LM5035

各位前辈好:
      我仿着TI的LM5035开发板做了一个半桥电源,原理图和下图类似:
         
       生产了30个样机,20个正常,10个异常。
       空载上电,就烧次级同步整流管Q4~Q7,Q4、Q5都烧毁了,Q4、Q5的门级有明显烧黑痕迹。Q6、Q7有的烧毁,有的还坚挺着。
       看上去,像是同步整流驱动电路短路,导致Q4、Q5门级烧毁,进而DS端短路,带着Q6、Q7一起短路。
       我怀疑是同步整流驱动问题,我去掉了Q4~Q7的驱动信号,就用体二极管整流,电路可以空载工作了。但一加上同步整流,就烧MOS。我怀疑是同步整流信号异常,可看了一个驱动波形又是正常的。很奇怪。
       还有一个怪现象,当只用体二极管整流时,我带了1A负载,电路也能工作,但是初级R3、R4之间的分压不均,不是Vin/2,而好的样机是分压均衡的。我量测了初级分压电阻和电容,阻值和容值无太大差异,我又量测了初级MOS驱动信号LO、HO,发现好的驱动信号一致,坏的驱动信号的占空比一大一小。我纳闷了,不知道是什么原因产生这种分压?由于分压不均,导致变压器次级8脚上的电压,也就是输出电感L2左端的电压也是一大一小,我现在只知道现象是异常的,但是找不到原因,又不知该如何排查?还请高手指点迷津,谢谢!