我使用TPS40055做一个输入18-36V,输出5V12A的电源,现在不带负载情况下,输出正常5V,带负载大概输出3A左右电压就掉到了4.6V左右,如果功率再高当达到7V左右,芯片就不能正常工作了。工作频率选的300K,电感选的4.7uH,mos管选的SIR836DP和SIR422DP。如果加负载后输出纹波峰峰值能达到2V左右,不带载纹波大概是100mv。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
首先确认功率电感饱和电流大于15A以上。
其次确认功率回路尽量小。
最好确认电流保护