最近用TPS65131芯片设计做一个模拟电路供电电源,电源输入电压为5V,输出为正负15V,当系统空载时能正常输出正负15V电压,当带上10片OPA2188运放后,输出正电压只有4.7V,无负电压输出了,且伴随有哨叫声,这是带不动这么多负载吗?不解,请大神帮助。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
根据OPA2188的手册说明,其静态工作电流最大才510微安,短路电流18mA,正常操作时工作电流应该在18mA以下,10块OPA2188加上外围电路一起工作电流应该在200MA以下才对。而TPS65131芯片手册上标明5V输入,正15V输出时电流可以达到550mA,负15V输出电流也能达到350mA,理论上不应该带不动才是。此款芯片s如果4.7UH电感频率范围不够,空载是否能正常输出?还请各位大神解惑