This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用XTR111输出无线性关系及器件损坏

Other Parts Discussed in Thread: XTR111

您好:

我们最近在使用TI得压流转换芯片XTR111,DAC输入0-5V,4-20ma输出,

Q4用的是MMBT5087,M2用的是BSP170P。VSP=23.7V,EF上拉为外接5V,OD置低,

SET为设置电阻1.65K, 最大输出电流量程为I=10x(5/1.65K)=30.3ma,

和demo板上的一样,PCB布局参照demo板布局。

现在测试。

PIN6为DAC输入4V

IS=23.7V

VG=5.0V,

SET为VIN电压

EE为低(负载开路,负载电压过大)?

晶体管发射极和基极之间的R15上无压降。

BSP170P的1为5V,,3脚为23.7V,现无负载输出23.7V,,外接1K电阻,电流为2ma, 均不受输入电压控制。

之前测试结果为,

4.9V-27ma

4.09V-22ma

3.09V-18ma

2.09V-损坏

1.09V-损坏

需更换晶体管,mos和IC器件。 

期待您得解答,谢谢、