This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3488升压升流

Other Parts Discussed in Thread: LM3488

3.7V锂电池输入,如何获得12V,3A可调电流或者电压,采用Datasheet的典型电路,在没有负载情况下电压是正确值,如果有负载情况下,电压只有6V左右,先咨询下,按照datasheet的典型电路,如何求电流问题???

  • Hi
    首先你要明确你是做恒流,还是恒压,这个要看你的负载。
    恒压比较好做,例如12V固定输出,电流由负载决定。
    带载能力下降,首先你要确定电感饱和电流是否足够,按照你3.7V电池,假设最低电压在3V左右,输出12V/3A, 效率85%, 电感饱和电流36/85%/3*1.2=17A, 这个电流相当大,电池能输出这么大,并维持吗?
  • 您好
    负载是4和个串联的3W的大功率LED管,现在目标是通过改变电压或者电流的方式,使其发光管能正常工作,正常工作状态下,电压典型值是2.2V~2.6V,单芯的电流是700mA,最大值是1A,现采用4个四芯灯珠串联,那边工作电压应该在8.8V~10.4V,最大可以达到11.2V将近12V,电路需要达到2.8A(典型值),故改变发光强度,那么电流范围应该在2A~4A可调,现拟采用3.7V锂电池供电,主要问题是如何改变反光管的亮度达到实验要求



    谢谢

  • 您好

    LM3488能做成恒流源吗?如果可以,该怎么设计呢???
    恒流源,电流3A左右哦,电压在8.8~12V可调,

    谢谢
  •  您好

    咨询下,一:Rsense,Rfilt,Cfilt选型基准是什么???作用是什么???
                  二:LM3488能设计成2~4A可调电流源???电压在10V左右,或者3A恒流源,电压8~12V

    谢谢

  • 四个LED串联,为什么电流还乘以4?
  • 您好

    因为每颗LED里面是四个灯芯(即单珠四芯),且四个灯芯是并联的,所以要乘以4