This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478 升压不稳定和启动不稳定

Other Parts Discussed in Thread: LM3478

这边再使用LM3478构建12V转36V电路时,出现芯片未启动和输出电压升高不稳定的情况。

1. 芯片未启动时,测量FA/SD引脚发现为7V~9V恒定电平,但是该引脚通过电阻接地,查阅LM3478手册发现该引脚传输方向只为输入,这是什么原因?

2. 输出电压升高不稳定时,设计输出电压为36V,电路会正常输出36V电压一段时间,之后开始输出不稳定高电压,此时输出电压在41V~60V之间来回变动,此情况在空载和接入负载的时候都有出现,这是什么原因?

  • Hi
    FA/SD有电压正常,外接电阻就是为了获得等值电流给内部电容充电做频率控制,但是如果电压是7V~9V就不正常,因为这个脚电压最大7V.
    其次输出电压异常偏高,注意反馈电阻选择的GND为模拟GND, 以及补偿电路配置。(模拟GND建议和功率GND分开),如果确认好没有问题,可以更换芯片看看,因为FA>7V是异常。
  • 因为我这边有好几片3478都出现了FA/SD引脚电压>7V,能否帮忙判断一下出现此类异常的原因?还有查阅手册DR引脚输出的驱动信号频率由FA/SD引脚的接地电阻确定,实际在使用过程将开关频率设置为130KHz时,会有出现输出频率为23KHz或者33Khz的驱动信号,这又是什么原因?