Hi TI,
项目上更改不带背光驱动屏;所以这次改板上使用LP8556TMX-E02来驱动15.6寸的屏(背光规格11串6并)的背光,由于屏的接口小板上没有预留I2C接口,此次LP8556的硬件连接只是接了PWM和EN/VDDIO pin,I2C和FSET & ISET都悬空,现在调试过程中发现LP8556不能升压,是否LP8556硬件连接必须要接I2C来控制,附件是电路图请帮忙检查,谢谢!lp8556_schematic.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI,
项目上更改不带背光驱动屏;所以这次改板上使用LP8556TMX-E02来驱动15.6寸的屏(背光规格11串6并)的背光,由于屏的接口小板上没有预留I2C接口,此次LP8556的硬件连接只是接了PWM和EN/VDDIO pin,I2C和FSET & ISET都悬空,现在调试过程中发现LP8556不能升压,是否LP8556硬件连接必须要接I2C来控制,附件是电路图请帮忙检查,谢谢!lp8556_schematic.pdf
Hi Johnsin,
因为我们现在选用的LP8566TMX-02,地址为A2h的默认配置为20h,其中的BL_ON脚为低表示02这颗是默认用I2C来控制;如果选用LP8566TMX-03,地址为A2h的默认配置为28h,这个表示默认为PWM控制,而且A2H的 ISEN_EN=0 ,BOOST_FSET_EN=0&PWM_FSET_EN=0;是否可以表示如果我们把IC换成LP8566TMX-03,就不需要I2C和ISET&FSET接下拉电阻,附件的电路图应该可以工作,不知道这样理解是否正确,还请帮忙确认,谢谢!