This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想咨询关于UCC256404的几个问题:1.软启动时间根据什么选择?2电流检测脚的延时电容怎么选?我现在遇到的问题是LLC可以带载启动,但是级联上PFC后,只能带60%负载可以启动,再高的话输出拉低,LLC一直处于重启状态?是不是和提到的这些参数有关,或者其它问题,PFC和LLC模块都是可以单独空载上电后带满载的,也可以带满载启动。就是级联就有问题。从哪些方面可以入手?谢谢
您好,是这样的,如果PFC正常启动,则可以正常的带满载启动,两者级联时不能带载启动的表现就是PFC输出电压一直在320V左右,这个电压是不能启动LLC的。
时序上这么解决?能说说您的建议吗?我目前做的实验包括减少isns电阻,增加与这个电阻并联的电容来增加延时;增加软启动时间10ms-20ms-40ms,最大时启动不起来LLC;增加VCC电容;增加PFC的带宽;在blk脚和FB加大滤波电容;目前都没有效果。观察isns脚在满载启动的波形如下图:ch1是RVCC ,CH3是ISNS,CH4是LO, ISNS电压是没有超过手册规定的的5V。
Hi
感谢分享。