This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131输出不正常,设计为±10V输出,实际正电压只有2.9V,负电压1.3V,可能是什么原因?

Other Parts Discussed in Thread: TPS65131

使用TPS65131的片子,设计为±10V的输出,使用电池供电输入电压3.6V,实际正电压只有2.9V,负电压1.3V。正电压输出对比输入电压,说明没有任何升压作用。

以下是分析过程,请大家帮助确认可能的原因是原理图,还是PCB设计,或者物料选择问题?谢谢!

1.电路图和PCB Layou设计t如下:

2.原理图中的boost和inverting converter的电阻值R109,R110,C128,R111,R112,C134都是参考规格书。

3.测量INP的管脚,有1.296Mhz的信号,峰峰值2.1V,最大电平3.94V,说明DCDC已经工作频率正常。

4.上传VIN管脚的波形,为3.6V电平,与输入电压相近。

5.下图是PCB照片: