This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询TPS53647+CSD95372BQ5MC电压源改为电流源的问题

Other Parts Discussed in Thread: CSD95372BQ5MC, TPS53647

你好!用TPS53647+CSD95372BQ5MC可以建立一个BUCK型恒压源,如果修改电路有关结构(和有关命令),不知是否能改为恒流源(比如50A最大电压是2V)?如果不能,利用TI公司有关元件是否可以构成一个恒流源(50A2V)

  • HI
    我觉得不好做,恒流和恒压的设计差别是反馈取样,但是这款芯片是多相控制,怎么电流取样呢? 电压取样方便是因为他们做同一个输出。
  • 在输出电路中有一个分流器,可以以产生一个75mV或100 mV的电压,然后通过运放,变成芯片所需要的参考电压。uc3525是相位180°的一组PWM信号。问题1:如果用两片UC3525,是否可以产生四路相位差是90°的PWM信号(固定频率)?或者直接有四路频率固定、相位差90°的PWM芯片。问题2:如果问题1都不能满足的话,能否提供一个三路相位差是120°的PWM芯片型号
  • Hi
    直接通过分流器,在总输出可以以产生一个75mV或100 mV的电压,然后通过运放给到反馈,这样做看看。
  • 参考上图,初步准备用一片UC3525产生两路相位是180°的PWM信号,然后通过CPLD可以产生四路相位是90°的PWM信号,然后用四个相位是90°的PWM信号驱动四个CSD95372BQ5MC。那么如果用UC3525+CSD95372BQ5MC, UC3525的震荡频率(F=1/(0.7Rt+3Rd)用多大比较合适?
    附仿真图形