This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

谈谈LLC谐振控制芯片UCC25600

Other Parts Discussed in Thread: UCC25600, UCD3138, UCC28600

          楼主的主要问题如下:现在想做一个150W的LED灯,准备做两级的,前级用BOOST升压,后级用一个LLC的谐振,输出大概是30V,想请教一下大家,做LLC谐振用哪一款芯片好?帖子链接:

http://www.deyisupport.com/question_answer/analog/power_management/f/24/t/58833.aspx

          TI FAE:,回答了楼主的问题,并且推荐了UCC25600,来实现LLC电路的控制。

         记得以前电源设计中经常使用的拓扑为RCC,正激,反激,半桥,全桥等电路,后来随着对电源的效率需求越来越高,LLC电路也逐渐普及起来,使用最多的芯片要数ST 的L6599了。再就是ON 的1397了。通过TI技术人员的介绍,我详细了解了一下UCC25600这个芯片的相关资料,在这里和大家一起分享一下使用UCC25600设计LLC电路的一点感悟,有不对的地方欢迎指正。

         首先,我们来看看UCC25600设计LLC电路的基本结构,如下图所示:

           UCC25600居然是8-Pin SOIC封装的!相比于L6599将近20脚的封装,体积小了很多,在PCB布局的时候,可以极大的节省空间。下面再来看看其典型的应用电路,也是相当简洁的。设计起来,方便多了。

           在这里顺便说一下,UCC25600设计LLC电路需要注意的几个方面的问题。从UCC25600的规格书中,我们可以了解到,UCC25600的外部结构虽然极其简单,但是该有的功能,可以说是一个都不少。

           我们先说说设计中需要注意的第一个功能,就是驱动电路的设计,从上图中,我们可以看出,LLC驱动是直接采用驱动变压器的,然后由UCC25600直接驱动。我们只是需要设计一个驱动变压器就行了。UCC25600的驱动能力为0.4A,下拉能力为0.8A。由于LLC是ZVS,所以并不需要很大的驱动能力,这个驱动能力完全满足一般的设计需求。

           在设计中需要注意的第二个问题,就是过流,或者短路保护。这个是电路设计中必备的。UCC25600提供的典型设计电路如下所示:

          过流短路保护,依靠谐振电容电压的半波采样,这个方式和L6599的保护方式基本一样,安全可靠。

          使用UCC25600设计LLC电路,还需要注意的一个问题,就是最高频率的设置,以及最低频率的限制,这个直接关系到LLC工作区间,以及可靠的保护功能的问题,十分重要。TI的官方推荐电路如下所示:

          正如小图所示,R1限制了最大工作频率。R2限制了最小的工作频率。关于其详细的计算方法,可以直接参考TI提供的 UCC25600的规格书。这里就不再介绍了。在设计中注意了以上几点,设计一个稳定,可靠,高效率的LLC电路就不再是问题了。

          如果你对LLC电路的设计还有其他的设计需求的话,还可以采用 推荐的数字控制方案UCD3138,专为电源量身定做的。

          以上就是使用UCC25600设计LLC电路的一点小体会,与大家一起分享下。欢迎讨论。