This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error: Sending Pattern LUT size failed!

Other Parts Discussed in Thread: DLPC900, DLP6500FLQ

在我们自己设计的DLPC900+DLP6500FLQ(无IT6535)系统中,调式出现如下故障:

1、加电后DLPC900运行正常,GUI运行也基本正常(如图),但“Internal Memory Test  Passed”没有勾选(没有通过?),DMD也没有显示预存Flash中的图像。

2、在“Pattern On-The-Fly Mode”模式,加载图片后,点击“Update LUT”,LED(D6)就停止闪了!过几秒钟GUI显示Error: Sending Pattern LUT size failed!,GUI程序也死了!

3、在“Video Mode”模式下选择“Internal Test Pattern”和“Checkerboard”,DMD没有任何显示,但程序没死 ,LED(D6)闪亮,DMD的电源(3.3V、8.5V、16V、-10V)都正常。

请问:

1、这个“Internal Memory Test”没有通过,是指DLPC900的还是DLP6500得?

2、问题主要出在DLPC900还是DLP6500?或者是接口连接上?

谢谢!