您好,
1,我用DLP4500外触发相机,投一张pattern相机拍摄一次,按照手册trig_out的引脚J14上的pin2接到了相机的触发线输入,pin6接的相机的地,但是用示波器显示J14的pin2输出,始终是3.2V或者3.4V,电平没有发生跳变,请问是哪里接线接错或者软件设置有问题么?
2,我想问一下如何拔掉usb线,dlp也能一直进行透射?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
感谢使用TI的DLP产品。
1,我用DLP4500外触发相机,投一张pattern相机拍摄一次,按照手册trig_out的引脚J14上的pin2接到了相机的触发线输入,pin6接的相机的地,但是用示波器显示J14的pin2输出,始终是3.2V或者3.4V,电平没有发生跳变,请问是哪里接线接错或者软件设置有问题么?
请检查DLPC350输出端的Trig_Out信号是否可以检测到跳变?
2,我想问一下如何拔掉usb线,dlp也能一直进行透射?
如果理解正确,是希望实现上电自动投射的功能。那么可以先按照需要配置好pattern序列,然后Save Solution ,将配置保存到.ini文件中,再将ini文件编译到固件中load到flash中,上电即可实现自动投图。
谢谢