在提出需求之前,想明确一个问题,我们希望开发DLPC150+DLP2010NIR的光谱平台,有个问题是,我们不知道如何check是否成功实现微镜的翻转。
问题如下:
1.请问,使用显微镜能看到DLP2010NIR的翻转状态吗?有更好的办法吗?
2.如果问题1没有好的解决办法,我们希望先开发一个投影的模块,以便熟悉DLPC+DMD的开发,能够给我们推荐一款与DLPC150+DLP2010NIR相近的在售投影模块吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在提出需求之前,想明确一个问题,我们希望开发DLPC150+DLP2010NIR的光谱平台,有个问题是,我们不知道如何check是否成功实现微镜的翻转。
问题如下:
1.请问,使用显微镜能看到DLP2010NIR的翻转状态吗?有更好的办法吗?
2.如果问题1没有好的解决办法,我们希望先开发一个投影的模块,以便熟悉DLPC+DMD的开发,能够给我们推荐一款与DLPC150+DLP2010NIR相近的在售投影模块吗?
您好!
感谢关注TI的DLP产品。
1. DLP2010NIR的微镜大小尺寸是5.4um,通常使用显微镜是可以看到镜子是否翻转的,但是微镜的翻转速度非常快,以60Hz输入,1bit情况下,1个状态的维持时间会在1ms以下。
2.与DLPC150功能类似的投影模块,可以考虑DLP2010EVM-LC,同时具有显示和pattern模式。
http://www.ti.com/tool/DLP2010EVM-LC
Best regards