好像该设备只支持900-1700 似乎不够用。我们想试试NIR 在纤维成分的检测应用上到底是否可行,各位有这方面的信息吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
好像该设备只支持900-1700 似乎不够用。我们想试试NIR 在纤维成分的检测应用上到底是否可行,各位有这方面的信息吗?
您好!
感谢使用TI的DLP产品。
DLP Nirscan Nano支持的波长范围是900-1700nm,上面使用的是DLP2010NIR,该芯片能支持700-2500nm,但是会有不同的光效。
Window Transmission Efficiency 96% Nominal (700 to 2000 nm, Single Pass Through Two Window Surfaces)
Window Transmission Efficiency 90% Nominal (2000 to 2500 nm, Single Pass Through Two Window Surfaces)
另外DLP NIRSCAN可以支持的波长范围是1350 - 2490nm,使用的是DLP4500NIR。
http://www.ti.com/tool/DLPNIRSCANEVM
Best regards