1、采用DLP进行微投影,如何选择合适的DLP的IC,需要从哪些方面考虑(这里主要是用作近红外成像图片),是否需要考虑前端摄像头的采集分辨率问题???
2、拟采用FPGA控制DLP投影,FPGA与DLP之间如何连接,采用什么通讯方式???
3、与DLP相连的前端光学元件如何选取?大小在2cm*2cm左右,有哪些公司在相应产品
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、采用DLP进行微投影,如何选择合适的DLP的IC,需要从哪些方面考虑(这里主要是用作近红外成像图片),是否需要考虑前端摄像头的采集分辨率问题???
2、拟采用FPGA控制DLP投影,FPGA与DLP之间如何连接,采用什么通讯方式???
3、与DLP相连的前端光学元件如何选取?大小在2cm*2cm左右,有哪些公司在相应产品
您好!
感谢关注TI的DLP产品。
根据您的问题:
1.目前DLP产品支持近红外的主要有DLP2010NIR(wvga)和DLP4500NIR(wxga),分辨率需要根据您的算法要求来确定
2.通常DLP芯片需要配合专门的ASIC芯片配合使用,比如DLP2010NIR需要与DLPC3470,DLP4500NIR需要与DLPC350配合使用,FPGA通过控制ASIC芯片实现对DLP的控制,数据接口通常是Parallel interface(RGB888),具体请参考ASIC的数据手册
3.使用DLP通常需要先搭建光学系统(光机),如下厂商可以提供现成的光机:
Best regards
您好!
1、我们产品主要应用在医疗方面的,静脉显影方向,不知道有推荐的IC可以参考吗?
->DLP2010NIR/DLP4500NIR/DLP3010等,需要根据您具体的需求来确定。
2、DLPC2607是与哪款DLP相对应呢???针对您回答的第二个问题,是否是可以理解成FPGA通过RGB88的通讯模式与ASIC(DLPC)相连,ASIC(DLPC)通过什么模式(LVDS???)与DLP相连,DLP与光机的通讯模式????
->DLPC2607可以搭配DLP2000,每一颗ASIC的数据手册中都会有介绍可以与之搭配使用的DLP。DLP通常是安装在光机中的,ASIC与DLP的通信不需要用户控制,ASIC会自动根据输入的数据与配置按照需要的时序发送给DLP。
3、现成的光机一般包含哪些东西???
->光机中一般包含了DLP芯片,光源,投影镜头,散热等,通常通过软排线与前端ASIC的板卡连接,也就是说客户可以只设计电子部分。
4、是否可以提供一些关于DLP的学习视频???
->请参考如下链接
Best regards