请问,
1.我们的DMD实际应用是曝光部分区域,但是微镜定时脉冲复位块操作,比如复位4块,需要的区域大于实际曝光区域。需要将复位块中的所有行数据全部刷新至DMD,再进行复位操作吗?
2.产品组中的软排线是安费诺的,关于软排线的长度,损耗方面,是否有相关限制,我们的应用是排线长度为600mm,安费诺没有这种规格的,所以我们自己定制,比较担心线长损耗
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
感谢关注TI的DLP产品。
请问具体需要使用的是哪个DMD芯片组?
从您的描述看使用的是DLPC410或者DLPC910,如果是,那么DMD的数据载入是按行载入的,需要保证一个行的完整,并不需要一个block全部刷新。比如:
https://e2e.ti.com/support/dlp/f/94/p/681190/2509757
在DLPC410或者DLPC910的数据手册中有关于走线的要求,比如线长,可以作为参考。
另外,请问您具体需要的应用是什么?
Best regards
您好!
1.需要使用随机模式,其他模式的ROW_AD(10:0)是不起效果的
2.各种复位的持续时间是相同的,具体取决于您的使用情况,The Global Reset duration is the same as the Single, Dual, and Quad Block Reset (MCP).
3.手册上给出的是推荐的最长长度,但是实际上有很多客户使用的长度超过了推荐的值,如果确实需要,您可以使用更长的走线。
Best regards