This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dlp4500 校准板的尺寸问题

版上各位好,有问题想请问大家
步骤是按照官方的手册dlpu019a.pdf进行
第一个问题 : 校准板的尺寸问题。
-在dlpu019a.pdf的第32页当中"The default chessboard size is 7 x 10"

可以看出校准板的格子数,由左至右(黑白都算在内),有10格没错,上到下是7格,这部分可以理解。

-不过问题出现了,"therefore the vertices of the squares on the grid, including the edges, will be 6 x 9."

想请问6 x 9是从哪里算出来的呢,谢谢?

第二个问题 : 校准板单一方格实际尺寸问题。

-在dlpu019a.pdf的第32页当中"For example, if each square is 2 cm wide, enter "2" into the prompt"

由于范例的方格的尺寸是"2 cm",可以在命令窗中输入"2"

不过我的方格尺寸是"0.9 cm",所以不晓得能否直接在命令窗中输入"0.9"呢,谢谢。

第三个问题 : 如果我希望点云距离单位可以更改,我想要输入更改尺寸的单位
例如 : cm 改成 mm ,需要从哪里设定呢?