This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010LC投影trig out 2曝光时间不对

Other Parts Discussed in Thread: DLP3010LC

Hi.

我司新项目使用的是新DMD: DLP3010LC

做板子参考的是TI官方的demo:TIDA-080003_DLP3010EVM-LC_DisplayBoard_SCH_RevB,使用的是DLPC3478+DLP3010LC+DLPA2005

未使用MSP430,只把mainboard上的CY7C65215与官方GUI进行通信控制加了进来。

目前的问题是:我在用TI官方的GUI 2.2.0.6进行internal patterns 进行设置好pattern sets后,点运行,用示波器看trig_out_2的曝光时间比设置的大,不一致。

设置了1500us曝光,但是示波器测量的是2000us。

具体设置的pattern set如下:

4个pattern set,全部是竖条纹1D。 第一个set有7个pattern, 第二个set有1个pattern,第三个set有1个pattern,第四个set有1个pattern。

按顺序进行投影,投影周期都是2500us,前暗时间500us,曝光时间1500us,后暗时间500us。     

请问是什么原因造成的?请验证回复。谢谢