This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

seed-sds650v2 链接 tms320c5517 弹出错误信息 -1063

C55xx: Error connecting to the target: (Error -1063 @ 0x0) Device ID is not recognized or is not supported by driver. Confirm device and debug probe configuration is correct, or update device driver. (Emulation package 6.0.14.5)

怎么处理,网上处理办法很少,用了也不成功。

  • 请问是自己的板子还是EVM板? ccs target configuration file里是怎么配置的?
  • 自己的板子
    配置文件用的是evm5517 ,seed xds560v2 usb Emulator
    Test Connection 输出以下内容:应当成功了,就是debug 会出 现错误
    [Start: SEED XDS560V2 USB Emulator_0]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -F inform,logfile=yes -S pathlength -S integrity

    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    C:\Users\wsqclock\AppData\Local\TEXASI~1\
    CCS\ti\0\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 560/2xx-class product.
    This utility will load the program 'seed560v2u.out'.
    Loaded FPGA Image: C:\ti\ccsv6\ccs_base\common\uscif\dtc_top.jbc
    The library build date was 'Sep 4 2015'.
    The library build time was '19:17:31'.
    The library package version is '6.0.14.5'.
    The library component version is '35.35.0.0'.
    The controller does not use a programmable FPGA.
    The controller has a version number of '6' (0x00000006).
    The controller has an insertion length of '0' (0x00000000).
    The cable+pod has a version number of '8' (0x00000008).
    The cable+pod has a capability number of '7423' (0x00001cff).
    This utility will attempt to reset the controller.
    This utility has successfully reset the controller.

    -----[Print the reset-command hardware log-file]-----------------------------

    The scan-path will be reset by toggling the JTAG TRST signal.
    The controller is the Nano-TBC VHDL.
    The link is a 560-class second-generation-560 cable.
    The software is configured for Nano-TBC VHDL features.
    The controller will be software reset via its registers.
    The controller has a logic ONE on its EMU[0] input pin.
    The controller has a logic ONE on its EMU[1] input pin.
    The controller will use falling-edge timing on output pins.
    The controller cannot control the timing on input pins.
    The scan-path link-delay has been set to exactly '2' (0x0002).
    The utility logic has not previously detected a power-loss.
    The utility logic is not currently detecting a power-loss.
    Loaded FPGA Image: C:\ti\ccsv6\ccs_base\common\uscif\dtc_top.jbc

    -----[The log-file for the JTAG TCLK output generated from the PLL]----------

    Test Size Coord MHz Flag Result Description
    ~~~~ ~~~~ ~~~~~~~ ~~~~~~~~ ~~~~ ~~~~~~~~~~~ ~~~~~~~~~~~~~~~~~~~
    1 none - 01 00 500.0kHz - similar isit internal clock
    2 none - 01 09 570.3kHz - similar isit internal clock
    3 64 - 01 00 500.0kHz O good value measure path length
    4 16 - 01 00 500.0kHz O good value auto step initial
    5 16 - 01 0D 601.6kHz O good value auto step delta
    6 16 - 01 1C 718.8kHz O good value auto step delta
    7 16 - 01 2E 859.4kHz O good value auto step delta
    8 16 + 00 02 1.031MHz O good value auto step delta
    9 16 + 00 0F 1.234MHz O good value auto step delta
    10 16 + 00 1F 1.484MHz O good value auto step delta
    11 16 + 00 32 1.781MHz O good value auto step delta
    12 16 + 01 04 2.125MHz O good value auto step delta
    13 16 + 01 11 2.531MHz O good value auto step delta
    14 16 + 01 21 3.031MHz O good value auto step delta
    15 16 + 01 34 3.625MHz O good value auto step delta
    16 16 + 02 05 4.313MHz O good value auto step delta
    17 16 + 02 13 5.188MHz O good value auto step delta
    18 16 + 02 23 6.188MHz O good value auto step delta
    19 16 + 02 37 7.438MHz O good value auto step delta
    20 16 + 03 07 8.875MHz O good value auto step delta
    21 16 + 03 15 10.63MHz O good value auto step delta
    22 16 + 03 1E 11.75MHz {O} good value auto step delta
    23 64 + 02 3E 7.875MHz O good value auto power initial
    24 64 + 03 0E 9.750MHz O good value auto power delta
    25 64 + 03 16 10.75MHz O good value auto power delta
    26 64 + 03 1A 11.25MHz O good value auto power delta
    27 64 + 03 1C 11.50MHz O good value auto power delta
    28 64 + 03 1D 11.63MHz O good value auto power delta
    29 64 + 03 1D 11.63MHz O good value auto power delta
    30 64 + 03 13 10.38MHz {O} good value auto margin initial

    The first internal/external clock test resuts are:
    The expect frequency was 500000Hz.
    The actual frequency was 499110Hz.
    The delta frequency was 890Hz.

    The second internal/external clock test resuts are:
    The expect frequency was 570312Hz.
    The actual frequency was 569976Hz.
    The delta frequency was 336Hz.

    In the scan-path tests:
    The test length was 2048 bits.
    The JTAG IR length was 38 bits.
    The JTAG DR length was 1 bits.

    The IR/DR scan-path tests used 30 frequencies.
    The IR/DR scan-path tests used 500.0kHz as the initial frequency.
    The IR/DR scan-path tests used 11.75MHz as the highest frequency.
    The IR/DR scan-path tests used 10.38MHz as the final frequency.

    -----[Measure the source and frequency of the final JTAG TCLKR input]--------

    The frequency of the JTAG TCLKR input is measured as 10.37MHz.

    The frequency of the JTAG TCLKR input and TCLKO output signals are similar.
    The target system likely uses the TCLKO output from the emulator PLL.

    -----[Perform the standard path-length test on the JTAG IR and DR]-----------

    This path-length test uses blocks of 64 32-bit words.

    || // -- \\ The test for the JTAG IR instruction path-length succeeded.
    The JTAG IR instruction path-length is 38 bits.

    The test for the JTAG DR bypass path-length succeeded.
    The JTAG DR bypass path-length is 1 bits.

    -----[Perform the Integrity scan-test on the JTAG IR]------------------------

    This test will use blocks of 64 32-bit words.
    This test will be applied just once.

    Do a test using 0xFFFFFFFF.
    Scan tests: 1, skipped: 0, failed: 0
    Do a test using 0x00000000.
    Scan tests: 2, skipped: 0, failed: 0
    Do a test using 0xFE03E0E2.
    Scan tests: 3, skipped: 0, failed: 0
    Do a test using 0x01FC1F1D.
    Scan tests: 4, skipped: 0, failed: 0
    Do a test using 0x5533CCAA.
    Scan tests: 5, skipped: 0, failed: 0
    Do a test using 0xAACC3355.
    Scan tests: 6, skipped: 0, failed: 0
    All of the values were scanned correctly.

    The JTAG IR Integrity scan-test has succeeded.

    -----[Perform the Integrity scan-test on the JTAG DR]------------------------

    This test will use blocks of 64 32-bit words.
    This test will be applied just once.

    Do a test using 0xFFFFFFFF.
    Scan tests: 1, skipped: 0, failed: 0
    Do a test using 0x00000000.
    Scan tests: 2, skipped: 0, failed: 0
    Do a test using 0xFE03E0E2.
    Scan tests: 3, skipped: 0, failed: 0
    Do a test using 0x01FC1F1D.
    Scan tests: 4, skipped: 0, failed: 0
    Do a test using 0x5533CCAA.
    Scan tests: 5, skipped: 0, failed: 0
    Do a test using 0xAACC3355.
    Scan tests: 6, skipped: 0, failed: 0
    All of the values were scanned correctly.

    The JTAG DR Integrity scan-test has succeeded.

    [End: SEED XDS560V2 USB Emulator_0]
  • 请问debug的时候出现什么错误?是先connect板子再去load .out文件的吗?
  • 点击debug按钮(小虫子),就连不上。提示:

    C55xx: Error connecting to the target: (Error -1063 @ 0x0) Device ID is not recognized or is not supported by driver. Confirm device and debug probe configuration is correct, or update device driver. (Emulation package 6.0.14.5)
  • 手动去connect板子,不要直接点debug按钮,看是否能成功连接板子。
    processors.wiki.ti.com/.../GSG:Debugging_projects_v5
  • 我最近购买了evm5517,因为我自己做的板子一直不能正常仿真。  我收到后,懵了。居然没光盘,只有板子和配件。也不知道到哪去问。能否告诉我,有配光盘吗?没有的话,怎么学习例程呢?

  • 有电话技术支持吗?
  • 这个链接里有学习的资料和例程.
    support.spectrumdigital.com/.../