我的系统是XP32位(虚拟机),从官网下载了CCS3.3,每次安装都是:安装到最后,安装进度条满了,就立刻死机。
虚拟机环境是VM14和VM15,XP的SP1和SP3都尝试过,现象完全一样(4个组合都试过,完全一样,折腾了好久了,求助)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
6840.ccs3.3-问题.mp4你好!在使用CCS 3.3 的时候遇到如下问题,希望得到你的帮助,谢谢!
IDE版本:ccs3.3.83.20
场景:使用simulator模式,没有连接硬件DSP。
逻辑:main函数中声明变量jTmp=0,在主循环中再赋值一次,jTmp=0。判断if(jTmp==0x12),if和else两个分支都进。
具体看附件中的视频