首先我添加了这两个库,但是编译出现这问题:
我已经在model选择 large,但我不知道这个file"-1"是什么。
接下来我添加了这个ax.lib
就出现这个问题
请问这样应该如何解决呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您看我一开始发的帖子第一条,就是没有a的lib的
我是新手,自己也不知道cmd文件怎么弄,我的cmd文件是在在general设置的,就图里这样
然后是我的cmd文件:
-w
-stack 1000
-sysstack 1000
-l rts55x.lib
-heap 1000h
MEMORY
{
DARAM: o=0x100, l=0x7f00
VECT : o=0x8000, l=0x100
STACKS: o=0x8100, l=0x1000
DARAM2: o=0xa100, l=0x5f00
SARAM: o=0x10000, l=0x20000
}
SECTIONS
{
.text: {} > DARAM
.vectors: {} > VECT
.trcinit: {} > DARAM
.gblinit: {} > DARAM
frt: {} > DARAM
.pinit: {} > DARAM
.sysinit: {} > DARAM
.csldata: {} > DARAM
.sysstack {} > STACKS
.stack: {} > STACKS
.bss: {} > DARAM2
.far: {} > DARAM2
.const: {} > DARAM2
.switch: {} > DARAM2
.system: {} > DARAM2
.cio: {} > DARAM2
.sysheap: {} > DARAM2
my_sec: > DARAM2
.cinit: {} > SARAM
}