在源文件中配置好了PLL,PSC,DDR2等一些参数,为什么在AISgen工具中还要配置,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
下面几个链接可以看看,说的比较明白。UBL= user boot loader,即二级boot。
A secondary bootloader, AKA User Bootloader (UBL), was required on older devices, where the bootloader could not parse AIS files. By using the AISgen tool with the OMAP-L138 bootloader, most of the functions previously performed by the UBL can be done instead by the bootloader.
For a typical Linux application, the old flow looked something like this:
The flow for the OMAP-L138 would look like this:
So in general, there is not a need for a separate UBL, as the AIS functions can perform most of the same tasks.