我目前使用的是CCS7.1,请问这个版本的CCS是否支持开发TMS320c6747,如果支持,我需要怎么搭建环境安装那些文件。
期待您的解答
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我目前使用的是CCS7.1,请问这个版本的CCS是否支持开发TMS320c6747,如果支持,我需要怎么搭建环境安装那些文件。
期待您的解答
谢谢!
我按照文档的操作安装了SDK,但是在CCS中编译SDK里的历程任然出现错误如下:
Description Resource Path Location Type
#1965 cannot open source file "ti/dsplib/dsplib.h" fft_example.c /FFT_Example_64P_LE_ELF line 51 C/C++ Problem
但是我已经安装了库同时自己也能找到这个文件,SDK和CCS安装路径均为默认路径。我如果手动将这个头文件添加进去之后,又会出现另一个错误:
Description Resource Path Location Type
#1965 cannot open source file "ti/dsplib/src/DSP_fir_gen/DSP_fir_gen.h" .ccsproject /FFT_Example_64P_LE_ELF line 38, external location: C:\ti\dsplib_c64xP_3_4_0_4\packages\ti\dsplib\dsplib.h C/C++ Problem
显示另一个头文件无法打开
请问这个是什么原因