This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我想请教一下tms320c6414 MCBSP配制为spi口的一些问题

请教一下,我现在需要使用MCBSP配制为SPI接口和大容量SPIFLASH通信。按照MCBSP配制为SPI的说明,一次片选有效最多发送32bit数据;但是现在S25FL512S的通信协议要求 一次片选有效发送内容为8bit指令+24bit或32bit地址+data,也就是说一次片选有效传输的bit位数会超过32bit。MCBSP配制的SPI无法满足要求。不知道上述理解是否正确?

如果正确,是否可以按如下我如下思路解决:

一、将MCBSP配制为GPIO,通关软件模拟SPI接口;

二、后续硬件改进为,FSX换为为DSP的GPIO口接到flash片选管教,仍然使用硬件配制SPI接口,只是使用软件控制GPIO口来模拟片选信号。