This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748使用C6748_StarterWare_1_20_03_03中的USB Bulk例程,USB通信过程中出现不相关的addrass

我需要一个USB Bulk设备来将数据传输到主机,但是我的老板不想使用RTOS,而是选择了C6748_StarterWare_1_20_03_03。

但是我遇到了一些问题。 我只需要一个USB Bulk设备,只使用endpoint0和1,但是运行lcdkC6748示例时,我的逻辑分析仪显示了三个设备。

我需要的设备的地址是59。 但是这里还有其他设备(地址:56、57)。 我知道设备地址每次都会改变,但是每次都会出现三个地址。

我查看了相关代码的结构体和中断程序,但没有找到如何删除不相关设备的方法(地址:56、57)。

请帮助我。

我是用的评估板的USB部分与lcdkC6748应该兼容。

时钟:24Mhz

CCS:5.5.0.00077

电路图如下所示: